• ADMV1014 Schematic and BOM Clarification

    Hi,

    Kindly clarify the difference in Schematic and BOM . The decoupling capacitor values do not match. attaching snap of same.

    Thanks, and Regards,

    Siddharth shah

  • ADMV1013 and ADMV1014 turn on

    Hi,

    I am using the ADMV1013


    First I turn on the device with a voltage of 5 V. Then I start the ACE software.


    After switching on, the blue light of the equipment turns on.


    And after about 40 seconds, the blue light starts flashing. the equipment automatically…

  • EVAL- ADMV1013 AND EVAL- ADMV1014 SUPPLY

    Hi,

    I am using the EVAL-ADMV1013


    First I turn on the device with a voltage of 5 V. Then I start the ACE software.


    After switching on, the blue light of the equipment turns on.


    And after about 40 seconds, the blue light starts flashing. the equipment automatically…

  • ADMV1014 maximum LO input frequency

    Hello

    In my application I would like to use the ADMV1014 LO port up 10.6GHz as it simplifies the design.   The datasheet states that the maximum LO is 10.25GHz.  

    The graphs in the datasheet seem to suggest that this configuration will be OK.  For instance…

  • ADMV1014 baseband DC output

    Hi,

    I would like to know the I/Q output voltage range using BB mode at 0Hz(DC).

    I only find a peak-to-peak voltage on page 32 of datasheet, but it only shows at -25dBm RF input power excluded DC.

    I want to use this value to paratice RF-to-Bits as followong…

  • ADMV1014 QUAD_FILTER settings

    Hello.

    The ADMV1014 datasheet shows 4 settings for the 4 bit QUAD_FILTER register, used to set the LO filter:

    Is it possible to use settings other than the ones shown in the table?    If so, what is the response for the other settings?

    No worries if this…

  • ADMV1014 Impedance Matching

    Hello,

    I have two questions relating to the return loss of the ADMV1014:

    1. The datasheet says the inputs and outputs are matched 50 ohm (or 100 ohm diff) - these look to be buffered based on the block diagram. Am I right that it is okay to put matching…

  • Why does ADMV1014-EVALZ have different band compared to ADMV1014? Is there any way to use 24GHz on the evaluation board?

    Hi.

    I am looking for a board that can down convert 24GHz - 24.25GHz.

    I have found the device, ADMV1014, and its evaluation board, ADMV1014-EVALZ.

    However, the evaluation board supports downconversion from 24.5GHz instead of 24GHz.

    I would like to know…

  • admv1014 eval save settings

    need to find a way to get the eval board to save settings or have a linux driver to talk to it to setup the settings. Any idea?

  • ACE does not recognize ADMV1014-EVALZ

    Hi all, 


    I have 9 ADMV1014-EVALZ but ACE (1.23.3085.133, 64 bits) does not recognize any of them. I installed the ACE ADMV1014-1014 plugin using the plug-in Manager, no problem.


    When I connect the ADMV1014 board to the computer using the USB, the system…