What is the correlation between 0dBFS for the ADMP521 and ADAU1761 digital input?
What is the correlation between 0dBFS for the ADMP521 and ADAU1761 digital input?
I am trying to drive a 521 using SPI hardware to drive the PDM clock (1Mhz) and capture pulses.
(Yes this is a hack but its been done before, see http://www.cypress.com/?app=forum&id=2232&rID=43249)
I can see variable PDM data come in when I…
Hi,
I am making measurements with the EVAL-ADMP521Z-FLEX using Clock: 1.78 MHz, Vdd=3.3v. I sample the PDM output bit train into a PC computer and make my analysis by S/W (I simulate a 4-pole LPF that produces signed 16-bit samples at 8.0 Ksamp/sec)…
Hi,
I've started a discussion in Beamforming with MEMS microphones. And now I want to use 256 microphones ADMP521 and 128
ADAU7002 (a new IC that can do PDM-to-I2S/TDM decimation) for beamforming application. So I will have 32 TDM8 lines. What…
MEMS microphone IBIS models by JeradL
IBIS models are now available for our MEMS microphones with digital interfaces - the ADMP421, ADMP521, and ADMP441. You can download these models through this link to Tools, Software, and Simulation Models. Check…
New MEMS microphone products by JeradL
We have recently released four new MEMS microphones, so I want to make sure that everyone is aware of them and highlight the key features of each.
This is a new digital microphone that has the widest dynamic…
Hello HonestEffort,
ADI sold off the MEMS microphone product line to Invensense so you can still find the ADMP521 but it is now called the INMP521.
Can you attach your project? There are some many ways that you can lose the signal that it will take…
Hi,
I want to create a beamforming system with more than 100 mics on a board. Now I think about using analog output MEMS mics like ADMP504. After mics I want to use simultaneously sampling multichannel sigma-delta ADC like TI ADS1278 for data capturing…
ADMP521 MEMS Dig mic.
Thanks