• About the evaluation board layout of EVAL-ADM7170

    Hello


    I would be grateful if you could have the data of the layout of the evaluation board of EVAL-ADM7170.
    I would like to know the VIA information of the heat dissipation pad.

    I would be grateful if you could reply.

    Best Regards,
    Knj

  • Load regulation of ADM7170

    Dear,

    I'm trying to simulate the load regulation of the ADM7170 to compare it with figure 4 of the ADM7170 user guide. However, the simulation result is showing a different result for V(out) in function of V(in), the curve in the user guide is going…

  • ADP5003 / ADM7170 design check

    I've been working on a power design using the ADP5003 and ADM7170.  I hope you will point out any flaws since I 've never done this before! Slight smile

    Topology: The design uses the adaptive mode of the 5003 where the buck drives the LDO, converting 5V to…

  • 关于LDO芯片ADM7170使用的问题。

    我想要使用ADM7170实现如下功能,输入电源电压+5V,输出电压+4.6V。查询ADM7170的手册使用其可调输出电压的参考电路设计,输出电压维Vout=1.2V*(1+R1/R2)。可是实际调试结果始终是输出5V电压,请问是什么原因呢?

  • ADM7170 - Vout 1.2 V

    Hi,

    I'm planning to use the ADM7170 as 1.2 V voltage source. According to the datasheet ordering guide table (page 23/23), the adjustable models (ADM7170ACPZ-R7 & ADM7170ACPZ-R2) are listed with an output voltage of 1.2 V.

    As stated on page 16…

  • 【本月重点推荐】CMOS、低压差(LDO)线性稳压器 ADM7170/1/2

    【本月重点推荐】CMOS、低压差(LDO)线性稳压器 ADM7170/1/2 by ADI_Amy

    CMOS、低压差(LDO)线性稳压器ADM7170ADM7171ADM7172,均采用2.3 V6.5 V电源供电,最大输出电流分别为500 mA1A2A 这三款高输出电流LDO均适用于调节6 V1.2 V供电的高性能模拟和混合信号电路。

    这三款器件均采用先进的专有架构,提供高电源抑制、低噪声特性,仅需一个4.7 μF小型陶瓷输出电容,便可实现出色的线路与负载瞬态响应性能。 对于1 mA至1…

  • Power Dissipation of ADM7170, ADM7171 and ADM7172.

    The data sheets for the ADM7170, ADM7171 and the ADM7172 all list the same thermal resistances even though their rated currents are 0.5A, 1.0A and 2.0 respectively. How can this be so if their maximum junction temperatures are all the same?

  • ADM7170

    Hello,

    I would like to use the ADM7170 with a voltage divider as shown in fig. 55 in the data sheet. I'd plan to use a DAC on the bottom of the divider with a 1nF cap to filter the DAC output. Is this acceptable or could it cause stability issues?…

  • ADM7170, ADM7171, ADM7172 soft start

    Is the soft start cap used to bypass the reference?

    Is there a max SS cap I can use?

    The description says also that SS needs to be left open when not used, but could the SS pin be used also as a REF in or Track function to lower the output voltage?…

  • 【本月重点推荐】CMOS、低压差(LDO)线性稳压器 ADM7170/1/2

    CMOS、低压差(LDO)线性稳压器ADM7170ADM7171ADM7172,均采用2.3 V6.5 V电源供电,最大输出电流分别为500 mA1A2A 这三款高输出电流LDO均适用于调节6 V1.2 V供电的高性能模拟和混合信号电路。

    这三款器件均采用先进的专有架构,提供高电源抑制、低噪声特性,仅需一个4.7 μF小型陶瓷输出电容,便可实现出色的线路与负载瞬态响应性能。 对于1 mA至1.5 A负载阶跃而言,负载瞬态响应通常为1.5 μs。

    ADM7170ADM7171