Hi there,
I have a question about ADM485, RS-485 transceiver.
http://www.analog.com/media/en/technical-documentation/data-sheets/ADM485.pdf
The datasheet says this device has fail-safe feature.
Could you be explain what is the fail safe feature of…
Hello
Our customer will use ADM485 and asks me about below.
Please let me know your advice.
ADM485 has receiver open fail safe.
So ADM485 has internal pull up resistor for fail safe.
If possible, could you give me about the value of internal pull…
Hi
I have a question ADM485 Propagation Delay.
If you have a Propagation Delay histogram data Driver and Receiver ,Please teach me.
Best Regards
HOD
Hi,
There is properly working kit
I need to increase the PCB power supply for ATmega8 up to …
Dear Sir
I have used an exception when using ADM485E communication. Some questions I would like to ask.
(1) ADM485E supports open fail safe function in RX mode in the datasheet, and the output is high level.
When all RS-485 driver is RX mode,the AB…
For MTBF calculations in accordance with MIL_HDBK_217F, I need the number of transistors (or MTBF/FIT) for the following devices:
ADuM3200
ADuM3201
ADR395
ADM485
Where it's possible to find this data? Can anyone help me?
Thanks
Giova…
is it safe to connect to RS-485 few ADM485 and ADM3485?
Some devices have Vcc=+3,3V and ICs ADM3485 are used for them,
some devices have Vcc=+5V and ADM485 are used.
hi
i have this circuit
and when i clear DE and RE pins output receive of adm485 make allot noise that make my MCU to RX overflow
is it normal or i should do something to fix it?
i forgot to put 100nF on VCC of it . cant it be the problem?
The differential input of ADM485 is pull up to 5V and pull down to 0V with 10k resistors and terminated with 120ohm resistor. If the RS485 bus is not connected the input voltage cross B and A is about 30mV (receiver is enabled and driver is disabled)…