ADM3491在进行RS422通讯时,接收和发送使能应该如何处理,数据手册的真值表里没给出来啊
Maximum Junction Temperature of ADM3491 is not available in datasheet. Please provide the same
I would like to ask how to implement half duplex in ADM3491? By shorting A to Y and B to Z?
Thanks all.
Ryan
Hello,
According to ADM3491-1 datasheet, this part " Meets IEC1000-4-4" as below,
What difference between IEC1000-4-4 and IEC610004-4?
IEC61000-4-4 covered IEC10004-4?
Thank you for your help in advance.
Best regards,
Sofy
这是我的电路图,485通讯时RXD1+和TXD1+以及RXD1-和TXD1-已跳线短接,使能置0,上位机485发送,下位机单片机就是收不到。一样的程序我直接单片机用串口TTL电平与电脑通讯可以的,求解释啊。
Hi Viacheslav,
Can you please explain the connection of the ADM3491 bus pins to the MOXA UPort 1130?
Is the ADM3491 wired up to the MOXA UPort 1130 correctly? Can you check the pin-outs?
And for R33 - what is the resistance value?
Regards,
Ric…
Hi Maxime,
The maximum Icc for the ADM3491 is about 70mA with 54 Ω loading at temperature 85C.
Richard
Hi,
ADM3491-1 is not recommended for new design rather than obsolete, as you could find more information here:Product Life Cycle Information
I cannot give you the accurate lifetime of this product but it should last at least more than 2 years.
Regards…