• ADM3488 termination

    Hello

    There are comment as below on the datasheet.

    "ADM3483/ADM3488 are more tolerant of imperfect termination."

    Is this meaning the termination resistor is not required?

    Regards,

  • ADM3488 ESD protection level

    Could you reply ADM3488 ESD protection level?

    What is ADLIB?

    Thanks,

    Kevin

  • ADM3488 - UART data output to a board with a biased logic level

    Hello,

    I am using the ADM3488 Transceiver on a board (Board #1) to transmit data to and from an FPGA which is on another board (Board #2). Board #1 is being powered by a 3.3V supply and Board #2 is operating off a 5V supply.

    There is a bias in the…

  • RE: Why the receiver output voltage low (VOL) is bigger than expected?

    Using one ADM3488 and one ADM3490 to feed the UART will get the VOL to about 0.85V, near the border of the accepted CMOS level. We did no testing with 2 ADM3488.

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…