• Explanation needed for power bypassing and power quality when driving a ADuCM355 from an ADM3260

    I am building an application that powers the ADuCM355 via isolated power from a ADM3260. I'm looking for a power supply topology and circuit that offers the most reliable and accurate operation for the ADuCM355.

    The ADM3260 datasheet is clear that…

  • ADM3260

    I'm using the ADM3260 in a new design.  VDD primary = 5V   Visol. = 5V The output level(SDA and SCL) at the line (isolated output) signal swing is 5V to 800mV. I have a 1k5 pull-up on both SDA and SCL. I've measured the output relative to the ADM3260…

  • ADM3260 ibis model

    Is there an IBIS model for the ADM3260 or a similar device that could be used. This is an Isolated I2C transceiver.

    Cheers

  • ADM3260: separate voltages for VIN and VDDP

    Hi,

    We plan to use the ADM3260 on a module. The module will be used in 3.3V, 5V and 3.3/5 mixed setups.

    The module hosting the ADM3260 breaks out VIN, GND, VDDP (& PDIS, SCL, SDA). Users of the module need to be able to power VIN and VDDP by separate…

  • RE: ADM3260 and ADE7953

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADM3260 performance in a two layer PCB

    Hello comunity, good morning/afternoon/night to all

    I saw this question in the forum but the answer was not clear.

    I want to know if it is possible to intergrate the ADM3260 in a dual layer design. The application I am working on is an isolated PH meter…

  • ADM3260 VSEL internal reference

    Hi,

    I would like to use ADM3260.

    So, I have two questions. Please help me.

    Question1:How about setting VISO?

    About the setting of VISO,

    Using Rtop and Rbottom resistors, is written in the data sheet.

    Depending on the values of the two resistors…

  • RE: Thermal Information of ADM3260 SSOP & ADE7953LFCSP

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADM3260 on 2 layer board, is it really possible?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADM3260 side1 and side2 logic levels definition

    Hello,

    After reading the datsheet of ADM3260 and ADuM1250, I'm a little bit confused.

    For the side1 of ADuM1250, it's compatible with I2C threshold, side2 is standard I2C logic levels and this is also the I2C bus side.

    For ADM3260, side1 and…