您好:
ADM3095E数据手册第3页中电源电流的描述令人困惑。
有两个问题:
1. 工作电流为8mA和90mA的两种工作条件是一样的吗?
2. 工作条件是No load的情况下,电源电流可以达到50mA和90mA吗?好像不正常。
期待您的回复。谢谢。
Hello,
I want to have a DO160G lighting protection in my board. "ADM3095E-EP" datasheets refers only DO-160G pin injection test waveform 3, 4/1 and 5A with level-4. But i want to know this device will support other test in DO-160G Section-22 like Cable…
On behalf of Richard Anslow:
The ADM2795E integrates an RS-485 transceiver, robust IEC 61000 EMC circuit, and digital isolation.
We also have the non-isolated ADM3095E. This integrates the same IEC 61000 EMC robustness as the ADM2795E, without the digital…
我的选择:
轻驾驶员停车难问题的智能监控系统
收发器ADM2795E和ADM3095E
Hi Sired,
We have a circuit note addressing your concern. I believe you will find it very helpful.
http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/CN0313.html#rd-overview
We also offer the mos…
Hi HS,
In that case for half duplex networks I would recommend these:
Kazu san, we need to clarify your requirements.
Do you mean "at least 64 transceivers" on the bus? (A part that allows 128 or 256 transceivers will work properly with 64 transceivers on the bus.)
By "5V and 3.3V" do you mean either one or the…
Sorry - I missed your follow-up question. I think it depends on the nature of your application, typically space-qualified parts will be radiation-tolerant or radiation-hardened; but there will be specific requirements to be fulfilled depending on system…
废话不多说,先放上官方微信二维码~(版主一向简单粗暴)
新年喜庆好礼带回家~拿出手机,扫描上方二维码即可参与“电路设计器件”讨论~就有机会参与抽取新年好礼哦~
版主现在就将ADI在2016年共推出数十款业界领先的集成电路产品罗列出,当然也欢迎跟帖讨论,讲讲你最喜欢哪款产品~你的设计中有什么有趣事儿都可以跟帖分享的哦~
更多ADF435…