• ADM3067E / ADM3068E

    Dear experts,

    My project needs a transceiver with 50 Mbs data rate so I thought about ADM3067E or ADM3068E.

    The question is:

    what is the minimum length of a cable to have that data rate? Is it possible to use a 5m  or 10m cable?

    I've read datasheet but…

  • RE: AD3067

    Hello, 

    Is the idea to use the ADM3067E as a repeater function? If this is in a point to point network or a multidrop network, you can permanently enable both the ADM3067E driver and receiver (by setting RE to GND and DE to GND). Any data received on the…

  • RE: ADUM6404 ISOLATOR FOR RS422 APPLICATION

    Hi Sandeep, 

    RS422 is a differential signal. The ADuM6404 has single-end I/O, and the levels are not compatible. 

    For RS-422 to RS-422 isolation (or an isolated repeater) we could use a non-isolated transceiver (ADM3067E for example) and an isolated RS…

  • RE: About the minimum pulse width of the receiver input of ADM3065E

    Hello Yuji,

    Thanks for showing your interest in one of our RS-485 Transceivers. The maximum data rate that can be achieved with ADM3065E is 50 Mbps, but it also depends on the other working conditions like the temperature and supply voltage.  If you're…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…