Hello,
I have 2 circuits which have the ADM3066E for Single-ended to RS485 translation.
I'd like to invert the logic so when circuit 1 transmits "high", circuit 2 will read "low", without changing the circuits.
Will it work well…
Hello,
I have 2 circuits which have the ADM3066E for Single-ended to RS485 translation.
I'd like to invert the logic so when circuit 1 transmits "high", circuit 2 will read "low", without changing the circuits.
Will it work well…
Using ADM306E 5Mbps I'd like to communicate by cable 20m.
But AN-960 When figure 7 is seen, there is 9.14m with the limit in 5Mbps.
Would there be any reform measures?
when VIO=ON,VCC=ON(Shutdown),DE=Low, is RO High-Z?
Hello Yuji,
Thanks for showing your interest in one of our RS-485 Transceivers. The maximum data rate that can be achieved with ADM3065E is 50 Mbps, but it also depends on the other working conditions like the temperature and supply voltage. If you're…
Hi HS,
In that case for half duplex networks I would recommend these:
Hi slavas,
We are in the process of updating the ADM3065E/ADM3066E data sheet. The branding will be added on the next revision. I apologize for any inconvenience.
Regards,
Richard
锵锵锵,最新中文资料赖来,快来收走吧~
系统方案精选APM
应用笔记 APPLICATION NOTE
参考设计 CIRCUIT FROM…
LTM2894
|
LTM2895 |
LTM9100 |
LTM2885 |
LTM2881 |
LTM2882 |
LTM2883 |
LTM2884 |
LTM2893 |
LTM2886 |
LTM2887 |
LTM2889 |
LTM2892 |
LTC1694-1 |
LTC4300 |
LTC4310 |
LTC4302 |
LTC4305 |
LTC4304 |
LTC4303 |
LTC4306 |
LTC4307 |
LTC4307-1 |
LTC430… |