• About input resistance of DE terminal of ADM3064E

    Hi,

    I am thinking of connecting the ADM3064E to the DE terminal from VIO (3.3V) via a resistor.

    In the data sheet, INPUT CURRENT is -2uA ~ 2uA,
    Is there a recommended value for the pull-up resistor between the DE terminal and VIO terminal?

    Also, please…

  • Pin wiring described in the ADM3064E data sheet

    I have a question about the connection destination of the AB.YZ terminal of the ADM3064E.

    In Figure 4 on page 1 of the data sheet, the connection destinations of the AB and YZ terminals are as follows.

    A: Non Invert
    B: Invert
    Y: Invert
    Z: Non…
  • RE: [RS485] Proudct selection advice needed

    Hello HS, 

    We have a few options available with a built in level shifter than operates down to 1.8V. 

    Your design looks to be full-duplex so I would recommend one of the following

    • ADM3064E (3.3V or 5V powered, enhanced ESD protection, for data rates up…
  • RE: About the minimum pulse width of the receiver input of ADM3065E

    Hello Yuji,

    Thanks for showing your interest in one of our RS-485 Transceivers. The maximum data rate that can be achieved with ADM3065E is 50 Mbps, but it also depends on the other working conditions like the temperature and supply voltage.  If you're…

  • 官方资料上线丨《数字隔离和接口技术选型指南2021》免费下载ing~

    “数字化”正在全球范围内掀起浪潮,推动科技如闪电般速度发展:数字医疗健康、电动汽车、 5G通信和智能制造……
    电子化器件中离不开隔离技术,而数字隔离凭借其更低的噪声和电磁干扰、更高的安全性以及更长的使用寿命,是隔离发展的必然趋势。
    ADI在数字隔离技术方面有着丰富的经验,iCoupler数字隔离可保护人员和财产免受高压影响,并保护关键数据免受破坏性电干扰。
    那么面对不同的应用领域,如何选择适合的数字隔离和接口解决方案以最大化加速您的项目?

    AD…