• ADM3057E VIORM definition

    Hi ADIExpert

    I have a ESS system as below functional block, one battery stack is composed of 14 series packs that provides voltage up to 1kV

    each battery pack is communicated with  master control board with iso CAN bus implemented by ADM3057E

    May I know…

  • RE: Reliability Data of ADM3055E and ADM3058E

    Hi,

    You can refer to ADM3057E (you will see some of the process data was actually gathered using ADM3055E) and for ADM3058E you can refer to ADM3050E (the same process is used for ADM3058E).

  • RE: Isolated interface chip with power supply

    Hi lijie,

    The ADM3055E and ADM3057E are isolated signal and power CAN FD transceivers. They are in SOIC packages.

    SPI signal and power isolation could be the ADuM5411 in SSOP, ADuM5401 or ADuM6421A in SOIC, if BGA solutions are not possible for this application…

  • RE: ADM3056EBRIZ - Isolated Power for VDD2

    Hi Selvaraj, 

    If there is not power available on the bus side, then an isolated power supply from the logic side will need to be provided. 

    The ADM3055E and ADM3057E have an integrated isolated dc/dc converter to supply the CAN FD transceiver. When there…

  • 系列第一弹丨ADI新品速递(2019 年 3 月)

    号外~号外~

    本着让筒子们拥有最佳体验的宗旨~ADI推出新产品新闻系列,让您能第一时间了解ADI本月新产品的介绍~

    话不多说,先上新产品新闻系列第一弹——3月新品~

    采用 6.25 mm × 6.25 mm BGA 封装的 12 A 15 A 引脚兼容型 μModule 稳压器将电感用作散热器

    ADI Power by LinearTM  20 VINμModule® (电源模块)稳压器 LTM4626 LTM4638 采用 3D