• ADM3056E CAN_H and CAN_L waveform

    Hi!

    I encountered some strange waveforms while evaluating the ADM3056EBRIZ: While the differential signal looks good (purple) and communication works, CAN HIGH and CAN LOW (green/yellow) seem very odd to me.



    This over/undershoot seems to be somewhat dependend…

  • RE: ADM3055E with dual power supplies

    Hi Kalexx, 

    The dc/dc converter is independant, and it would be possible to power only the VIO and VISOIN pins for a fully functional isolated transceiver. The VISOIN pin needs a 5V supply. 

    It may make more sense to use the ADM3056E though. That is the…

  • RE: ADM3054 Common Mode Voltage

    Hi Guy, 

    The ADM3054 transceiver can tolerate a +12/-7 common mode range. The figure is perhaps a bit hidden in Table1's test conditions of the receiver specifications in the ADM3054 datasheet. 

    The latest generation of signal isolated CAN FD transceivers…

  • RE: ADM3054 Input Waveform for CANH/CANL

    Hi Akira, 

    What is the configuration of the bus and location of terminations? 

    If this project is in the prototype phase, they could consider an isolated transceiver like the ADM3056E which has an RS pin. The slope control mode will reduce the slew rate…

  • ADI 新品速递(2019 年 5 月)

    ADI 5月新产品上线,想了解的筒子们不要错过!

    0.5 dB LSB6 位硅数字衰减器,9 kHz 40 GHz

    ADRF5720 是一款 6 位数字硅衰减器,以 0.5 dB 步长提供 31.5 dB 的衰减控制范围。该器件的工作频率范围为 9 kHz 至 40 GHz,提供优于 4.5 dB 的插入损耗和出色的衰减精度。在所有状态下,ADRF5720 的 ATTIN 端口具有 27 dBm(平均值)和 30 dBm(峰值)的射频 (RF) 输入功率处理能力。

    主要特性

    • 超宽带频率范围…
  • 21合1,ADI新品年底大盘点来啦

    转眼间,桌上2018年的日历就已经撕到了后一张。

    蓦地回首,才发现,斑竹竟然还没计划今年的新品盘点,惭愧惭愧~

    不过万幸,总算是及时记起来了。

    今天斑竹就来盘点下2018年ADI发布的那些重量级新品,绝对值得你关注~

     

    业界首款混合式降压型同步控制器LTC7821

    LTC7821把开关电容器电路与一个同步降压型控制器相结合,可使 DC/DC 转换器解决方案尺寸相比传统降压解决方案锐减 50% 之多。这种改善是通过将开关频率提高 3 倍实现的 (并未牺牲效率)。或者,当工作于相同的频率时,基于…

  • 超全产品合集丨ADI 2019年度硬核新品大集结,码起来慢慢看!

    马上就是农历新年,在2019年里你都做了些啥呀~而ADI为了满足各位工程师不断变化的设计需求,从没停下新品发布的脚步。今天斑竹为大家盘点下2019年来ADI发布的硬核新品,看看咱们ADI工程师这一年来杠杠的成果吧~

    小尺寸、高效率、低噪声、单片同步 4A 降压型 DC/DC 转换器 LTC3308A 

    LTC3308A 采用 2.25V 至 5.5V 输入电源,在高达 3 MHz 的开关频率下使用恒定频率峰值电流模式控制,最短接通时间低至 22 ns,可通过小型外部元件实现快速瞬态响应。Silent Sw…

  • 官方资料上线丨《数字隔离和接口技术选型指南2021》免费下载ing~

    “数字化”正在全球范围内掀起浪潮,推动科技如闪电般速度发展:数字医疗健康、电动汽车、 5G通信和智能制造……
    电子化器件中离不开隔离技术,而数字隔离凭借其更低的噪声和电磁干扰、更高的安全性以及更长的使用寿命,是隔离发展的必然趋势。
    ADI在数字隔离技术方面有着丰富的经验,iCoupler数字隔离可保护人员和财产免受高压影响,并保护关键数据免受破坏性电干扰。
    那么面对不同的应用领域,如何选择适合的数字隔离和接口解决方案以最大化加速您的项目?

    AD…