Hi all,
Does ADM3055E comply with ISO11898-3:2006?
Hi all,
Does ADM3055E comply with ISO11898-3:2006?
Dears,
How to get ADM3055E and ADM3058E Reliability Data High Temperature Operating Life (HTOL), Failures in Time (FIT), Mean Time to Fail (MTTF)?
the web link https://www.analog.com/en/about-adi/quality-reliability/reliability-data/wafer-fabrication-data…
Thank Jason. It is a bit difficult to buy ADM3055 at present, so I use ADM3055 temporarily. Can I recommend a TVS for ADM3053?
Hi farah.mim,
The ADM3054 is not a CAN FD isolated transceiver. The top speed is 1Mbps.
Check out the ADM3055E for CAN FD up to 12Mbps
www.analog.com/ADM3055E
Or the LTM2889 for CAN FD up to 4Mbps
www.analog.com/LTM2889
Regards,
Jason
ADM3053 has no minimum baud rate, because it has no "dominant timeout" (it won't bring CANH/CANL recessive even if TXD is still held low for a long time). The part will operate normally even at very low bit rates.
If dominant timeout is…
Hi tbob,
The EVAL-2LCANRS485EBZ may be a helpful example. Its a two port (CAN & RS485) board that demonstrates layout techniques with the ADM3053 and ADM2582E. This board meets Class A. Emissions scans are available in UG-1561.
Hi Rajeev,
1. Whether separate isolated power supplies should power the VCC and VIO Pins?
Having isolated supplies for VCC and VIO would not be useful. On the logic side, the isolated dc/dc converter and signal isolator share a gnd paddle; So isolated…
Hi lijie,
The ADM3055E and ADM3057E are isolated signal and power CAN FD transceivers. They are in SOIC packages.
SPI signal and power isolation could be the ADuM5411 in SSOP, ADuM5401 or ADuM6421A in SOIC, if BGA solutions are not possible for this application…
CAN-FD does have additional requirements for compliance to this new standard, although Classic CAN nodes such at those using ADM3054 may be compatible.
To implement CAN-FD using ADI transceivers, we recommend the newly released ADM3055E, which has integrated…