• ADM3054 Common Mode Voltage

    Hi,

    I'm looking at the ADM3054 isolated CAN transceiver and I did not find the common mode voltage specification for the bus side. To clarify the spec I am looking for: the max voltage of CANH or CANL measured in reference to GND2, that still allows…

  • ADM3054 Input Waveform for CANH/CANL

    Hello,

    I have a question about a input waveform of ADM3054 from my customer.

    Are there any problem when we input like a following figure waveform to CANH/CANL of ADM3054? It has large overshoot. The customer has no connection problem. He would like to…

  • ADM3054 power consumption

    How to estimate the power consumption of the ADM3054 when the communication rate is low.

  • CAN FD on ADM3054 transceiver?

    Hello,

    There are no informations about the CAN FD on the datasheet.

    I need to know if ADM3054 can meet the CAN FD required?

    Thanks for your help.

  • RE: ADM3054 Comm fail

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADM3054 1MHz Emission fails

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADM3054 bit rate problem

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Footprints of ADM3054/2487/2483

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADM3054 can meet the CAN FD required?

    CAN-FD does have additional requirements for compliance to this new standard, although Classic CAN nodes such at those using ADM3054 may be compatible.

    To implement CAN-FD using ADI transceivers, we recommend the newly released ADM3055E, which has integrated…

  • Power up for VDD1 and VDD2 pin of ADM3054

    VDD1 and VDD2 pin of ADM3054

    Hello

    I have 2 questions for ADM3054 from the customers .

    1: Do you have recommended operation for VDD1 and VDD2 sequence?
    My assumption is as follow.
    Is this right?

    If they need to monitor VDD2 SENSE:
    It is recommended to power…