Do you provide any Linux CAN driver support along with this ADM3051 IC?
For using a non - CAN tx - rx GPIO configuration.
Regards,
Saravanakumar
Do you provide any Linux CAN driver support along with this ADM3051 IC?
For using a non - CAN tx - rx GPIO configuration.
Regards,
Saravanakumar
Hi, support team.
Please tell me the configuration of the protection circuit of ADM3051.
To protect CANH/CANL from ± 36V , Is there a protection element other than attached circuit?
Best regards,
Hi
I have a question ADM3051 Maximum Ratings.
In customer's usage state, -1.3V/40ns is impressed on a TxD terminal and a RS terminal.
ADM3051 Maximum Ratings
The under chute hours are 6ns and instant-like.
When mean voltage is considered as…
Device : ADM3051.
Please teach me the rating of RXD the sink current.
I would like to drive the photocoupler using the H/L of RXD.
Insert the resistance, drive current of the photo-coupler is 10mA.
So RXD pin,Current is 10mA sink.
I attach a rough i…
Post-Thanksgiving we're grateful for our members and forum managers for providing quality solutions to your toughest challenges. So far in 2021, we saw the biggest spike in membership and an increase in member engagement compared to the previous year…
Hi Keven,
Yes if it is based on classic CAN. The ADM3051/2/3/4 transceivers comply with ISO11898 for classic CAN.
Regards,
Jason
Hi Kannan,
When comparing the ADM3053 current consumption, the MCP2551 or other non-isolated CAN parts are not the best match. The ADM3051 is our non-isolated CAN transceiver best match.
For example;
ADM3051 NON-ISOLATED CAN TRANSCEIVER
Supply current…
Hi Ultraviolet919,
Yes, it should be possible to implement back to back ADM3053/ADM3053, connecting the logic I/O pins TX and RX together.
As such, you are creating an isolated CAN repeater node.
In a previous post, one customer used ADM3053 + ADM3051…
Hi Divya,
The ADuCM360 has UART but not CAN interfaces. Some options: