FAQ
Dear All:
ADM2484E Pin7 & Pin 10 is NC pin ,TI ISO3080 show GND1 & GND 2 ,But ADM2484E datasheet Pin7 & Pin 10 description "No Connect. This pin must be left floating." if mount ISO3080 PCB Layout have any question ??
Best
Ja…
Hi
I have a question ADM2484E.
ADM2484E DS is write,
'The logic side of the device can be powered with either a 5 V or a 3.3 V supply, whereas the bus side requires an isolated 3.3 V supply.'
And ,
Vdd2 ABSOLUTE MAXIMUM RATINGS is 6V max…
I would like to know if the ADM2484E compliant with IEC 61010-1 (2010-6).
Hi
I have a question ADM2484E.
ABSOLUTE MAXIMUM RATINGS "Bus Terminal Voltages - 9 V to + 14 V"
Which terminal voltage will be the next?
In case of
① Voltage for each of Y-GND 2, Z-GND 2, A-GND 2, and B-GND 2
② Voltage for each of Y - Z and…
Hi
I have a question ADM2484E ABSOLUTE MAXIMUM RATINGS.
Bus Terminal Voltages is -9V to 14V.
In this time , VDD1 and VDD2 is it necessary? or Is it unnecessary?
Best Regards
HOD