Hello,
I'm having an issue with an ADM2483 not doing full 'swings' on the RxD line....
I have two ADM2483 side by side, one with an isolated bus power supply of 5V, and one with an non-isolated power supply of 5V. The non-isolated module…
Hello,
I'm having an issue with an ADM2483 not doing full 'swings' on the RxD line....
I have two ADM2483 side by side, one with an isolated bus power supply of 5V, and one with an non-isolated power supply of 5V. The non-isolated module…
Hello,
About PV pin of ADM2483
Has internal pull-up resistors to the PV pin?
If pull-up resistance are incorporated, the number of value ?
Let me tell your advice.
Best regards,
Hello,
About PV pin of ADM2483,
Does user should do something for unused PV pin? or can leave NC?
Datasheet does not say any recommendation for unused PV pin. So I suppose that PV pin can leave NC(open).
Let me tell your advice.
Best regards,
…I found that ADM2483 has a PV input pin and ADM809 is recommended to drive this
pin. If I want to use this function, can I tie it to microcontroller to temporary isolate TXD/RXD pins from RS-485 traffic?
Hi ,everyone:
I use one ADM2483 chip with 1W isolated power (BS0505S-1W).Now I want to use five ADM2483 chips on one PCB,so should I how to choose the isolated power value ?
Thanks!
Hi 大家好:
现在使用ADM2483芯片来做RS485收发器,隔离电源采用金升阳BS0505-1W模块,现在一块电路板想支持5路485电路,使用5片ADM2483芯片,请问需要多大功率的隔离电源比较合适?
谢谢大家!
Does ADM2483 is tolerant until a noise of what V?
Thank you.
Are the NC pins on the ADM2483 internally connected?
More specifically, to maintain compatibility with an existing layout is it acceptable to connect pin 10 (NC) with pin 9 (GND2)? Will this affect isolation or transient ratings?