• Question about ADM202E and ADM1181A

    Hi,

    I have two questions about the doubler operation of them.

    Please check the attachment and take care of this case.

     PDF

    Regards,

    Kazu

  • RE: ESD protection for ADM232A

    Thank you for your query, 

    The ADM232A has 1500V protection to the Human Body Model (HBM) standard on all pins.


    The ADM202E is a suitable alternative with 15kV ESD protection on the RS-232 pins, to the system level IEC61000-4-2 standard.
    https://www.analog…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • (AD8206/AD8211)Why did you change the datasheet?

    Hi !

    I have some questions about ADI datasheet.

    Our team are checking the datasheet because if the datasheet was changed we have to explain the changes.

    And today , we found many datasheet was changed.

    For just one example , AD8206 datasheet was changed…

  • Extra power supplies for Active Learning Modules (M2k , M1k)

    Extra power supplies for Active Learning Modules (M2k , M1k)

    We have over the years gotten many questions with regard to the limited current and voltages available from the built in user power supplies provided by the Active Learning Modules ADALM1000…

  • 官方资料上线丨《数字隔离和接口技术选型指南2021》免费下载ing~

    “数字化”正在全球范围内掀起浪潮,推动科技如闪电般速度发展:数字医疗健康、电动汽车、 5G通信和智能制造……
    电子化器件中离不开隔离技术,而数字隔离凭借其更低的噪声和电磁干扰、更高的安全性以及更长的使用寿命,是隔离发展的必然趋势。
    ADI在数字隔离技术方面有着丰富的经验,iCoupler数字隔离可保护人员和财产免受高压影响,并保护关键数据免受破坏性电干扰。
    那么面对不同的应用领域,如何选择适合的数字隔离和接口解决方案以最大化加速您的项目?

    AD…

  • ADuC7XXX系列常见问题解答

    问题:ADUC7XXX系列的开发方法和开发工具是怎样的?

    答案:ADuC7XXX的开发方法是非常简便的。ADUC7XXX系列提供了三种评估板套件,以帮助用户熟悉ADuC7XXX的开发方法和开发环境。以ADUC7020和ADUC7026为例,一种是EVAL-ADuC7020MKZ,这是一种迷你套件,它包括一块迷你评估板,电源线和串行下载线;另一种是EVAL-ADUC7026QSZ,它包括一块评估板,9V电源,串行下载线,和相应的软件光盘;还有一种是EVAL-ADUC7026QSPZ,它与前一种的区别是包括了一个硬件仿真器…

  • RE: ADuC7023燒入問題

    建议您参照附件的11页逐一排查