• RE: ESD protection for ADM232A

    Thank you for your query, 

    The ADM232A has 1500V protection to the Human Body Model (HBM) standard on all pins.


    The ADM202E is a suitable alternative with 15kV ESD protection on the RS-232 pins, to the system level IEC61000-4-2 standard.
    https://www.analog…

  • (AD8206/AD8211)Why did you change the datasheet?

    Hi !

    I have some questions about ADI datasheet.

    Our team are checking the datasheet because if the datasheet was changed we have to explain the changes.

    And today , we found many datasheet was changed.

    For just one example , AD8206 datasheet was changed…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • soldering temperature and soldering time

    We are using ADM202EARUZ-REEL but we can not find its soldering temperature and
    soldering time.

     

    We only have the Maximum soldering temperature and soldering time on datasheet.
    ADI advises reflow profiles should conform to J-STD 20 from…
  • Extra power supplies for Active Learning Modules (M2k , M1k)

    Extra power supplies for Active Learning Modules (M2k , M1k)

    We have over the years gotten many questions with regard to the limited current and voltages available from the built in user power supplies provided by the Active Learning Modules ADALM1000…

  • ADuC7XXX系列常见问题解答

    问题:ADUC7XXX系列的开发方法和开发工具是怎样的?

    答案:ADuC7XXX的开发方法是非常简便的。ADUC7XXX系列提供了三种评估板套件,以帮助用户熟悉ADuC7XXX的开发方法和开发环境。以ADUC7020和ADUC7026为例,一种是EVAL-ADuC7020MKZ,这是一种迷你套件,它包括一块迷你评估板,电源线和串行下载线;另一种是EVAL-ADUC7026QSZ,它包括一块评估板,9V电源,串行下载线,和相应的软件光盘;还有一种是EVAL-ADUC7026QSPZ,它与前一种的区别是包括了一个硬件仿真器…