• ADM1293 Power monitor read value

    Hello,

    I am using TES ver0.16 with ZCU102 and ADRV9002.

    I am trying to use Power monitor by changing the C99 example code.

    The changed code is as follows.

    #include <inttypes.h>
    
    #include "adi_adm1293.h"
    #include "adi_adm1293_hal.h"
    #include "adi_adm1293_types…

  • ADM1293

    I am new at using the ADM1293. When I put a load of 15A, I read back 13A. Is there a way to calibrate this so the load used is very close to the reported value?  What is an acceptable error?

  • ADM1293 Peripheral circuit configuration

     we encounter an application problem  when we use adM1293.  there is a big difference between the two schemes;

    As described below;

    1   R1, R37 use 10ohm, C4 use 10nf; C2, C3 remove , ADM1293 value  of  current sense  is unstable; the scheme  is your recommended s…

  • ADRV9002 Eval board - ADM1293 Power monitor function for C code implementation

    Hi,

    I would like to monitor ADRV9002 power consumption from on board ADM1293. TES power monitor function is not enough time scale and resolution. So, I would like to try to read it by C code implementation.(Use C code generation function and TES SD card…

  • RE: ADM1293 GENERATING AN ALERT

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADM1293 I2C hold time

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADM1293 Delta Power negative issue

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • What are the min and max sample rates for the ADM1293-1 over temperature?

    Hello,

    What are the min and max sample rates for the ADM1293-1 over temperature? 

    We are trying to decide if we can use the normal EIN Read or if we have to use the extended read.  We do not wish to do any averaging.

    The data sheet gives an example of 8236…

  • RE: ADRV9002 ZCU102 TES Connection Failure

    Hi, 

    Interesting, we have started using port 55558 in recent TES versions for the power monitoring data from the ADM1293. It might be worth adding the exceptions to that port too? 

    Regards

  • RE: High side current measurement

    Hi Htek,

        There are probably several dozen different ways to do this. Since you want to receive the value in digital form, I suggest that you use one of our high side current monitors. Take a look at these:

    LTC4151 High voltage I2C voltage and current…