• ADM1272's ISTART current limit and Start-Up CB(circuit breaker)

    Dear ADI Expert,

    What is the difference between ADM1272's ISTART current limit and Start-Up circuit breaker?

    Thanks.

    Best regards.

    Andy Yang.

  • ADM1272 ENABLE issue

    Hi ADI

    We have use ADM1272 for 54V hotswap, but there has a problem that it can't be re-start when ENABLE is triggered.
    Here’s the condition below while occurring fault, could you help to analyze what happened?
    Test method: like warm boot at system…

  • ADM1272 I_Set

    Hi , I have some problems for ADM1272 Eva-Board. I calculated resistance values for I_SET. These resistance values are 100Kohm (Vcap to Iset) and 226Kohm (Iset to GND)  I want I_SET = 1.9 volt. Therefore , It will be V_SENSE= 20mV and Current limit = 20…

  • Does the ADM1272 require a minimum output capacitor?

    Dear Sir,

    My customer is now testing their own ADM1272 board. Some ADM1272s are not designed with output capacitors. Testing is a bit problematic now. The test with output capacitance is normal. As shown in the first picture. The test without output capacitance…

  • ADM1272 pins values

    Hi ,

    ADM1272 datasheet isnis clearly to understand. For example, I did not understand E_fault and E_start pins. Is there any design tool this hot swap ?

    Thanks a lot.

  • ADM1272 Estart&Efault Pin

    Hi ,

    I have a ADM1272 Eva Board. It is not clearly information related Estart and Efault pins. The subject has been opened before. But nothing has been explained. Which formulas are applied here? Thanks for your help.

  • What different between Istart and Inrush current for ADM1272?

    Hi ADI Expert,

    I am confused about this.  What different between Istart and Inrush current for ADM1272?

    Thanks.

    Andy Yang.

  • ADM1272 Reading Vout Value

    Hi All,

     I am using ADM1272's evaluation board(EVAL-ADM1272EBZ). I am trying to code PMBus interface via VHDL. I want to read the Vout value for a specific application but I can't. According to datasheet, there are some procedures for reading Vout. I followed…

  • ADM1272 custom MOSFET & Rsense footprint

    Dear Sir,

    My customer is designing new project using ADM1272, might I request for ADM1272 EVM's footprint & dissension as below ?

    Thank you!

    Henry