手册说这个管脚电压默认拉高,请问大概电压是多高,是输入的Vcc,还是我外接上拉电阻的那个电压?因为要把这个管脚连接到处理器,怕电压过高打坏后级电路。
希望高手指导!!
手册说这个管脚电压默认拉高,请问大概电压是多高,是输入的Vcc,还是我外接上拉电阻的那个电压?因为要把这个管脚连接到处理器,怕电压过高打坏后级电路。
希望高手指导!!
I'm working with ADM1191 but I can not read voltage data.
I use Cora z7 to act as master, and use ADM1191 to read voltage of pi-fan.
In this case, I use 0x60 to be slave address.
Here is my code,
IIC::ConfigTable write_Config[4] = {{0x83,0x00}, …
Hello,
We would like to design the ADM1191 for POL power monitor application.
So far I have three question for this schematic
1. SETV pin, if we dont need to setting the alertb, may I floating this pin or any suggestion for this connection.
2. About…
Hi,
I want to use ADM1191 in only voltage readback mode.
In that case do we really need Rsense and setV connections??
pls clarify.
Regards,
Sandeep Jain
hi there .
i plan to use adm1191 monitor to measure another chip's input voltage and current . and my teacher request a theoratical analysis . i got 2 questions while reading the datasheet:
1. the voltage supply of 1191 ranged from 3.15V to 26V…
Hello.
I use ADM1191 as a power meter (voltage and current) for motor control application. I init IC to continious convert both voltage and current, or voltage only, or current only. MCU reads values by I2C but returned voltage is less than measured…
I'm using 3 ADM1191 to monitor the voltages and currents on my power amplifier FETs (see below). I've set up the devices to read continously and poll the values. They work as expected, except at about -10 deg C, 2 of the 3 devices sometimes start giving…
小弟我是一个尚在学习过程的学生,现如今试图用ADM1191芯片测试其他电路的电流, 有两个问题想要请教:
1、ADM1191本身芯片电源为3.15到26V,是否意味着SENSE端只能测试接近这个范围的电压?
2、数据手册的第13页右方写着对其12BIT寄存器寄存的电压值的读取,公式给出的Vfullscale=6.65Vor26.52V 是否意味着要达到fullscale必须要用这两个电压才可以?如是,那若我要测其他范围的电压要如何调整其量程?如不是,我该怎么理解数据手册上这部分的内容?
小弟明白这些问题比较粗浅…
Hi Htek,
There are probably several dozen different ways to do this. Since you want to receive the value in digital form, I suggest that you use one of our high side current monitors. Take a look at these:
LTC4151 High voltage I2C voltage and current…