使用ADM1185监控3路电源(3.3V、1.8V、1.2V)时,-40℃~-10℃环境下,有板卡Powergood输出为低,下图是原理图,
故障时,3.3V、1.8V,1.2V电压都正常,与正常板卡对比,上电时序也无差异。
1.8V和1.2V都是LDO
不知道怎么进一步往下分析了,不知道ADM1185的设计是否有问题?
what's the package weight of ADM1185 ADM1068 and ADM1065?
The PWRGD pin in ADM1185 is open drain output, the rise time will depend on the pull resistor that you are using for the output and the trace capacitance.
I don't know if it's needed, but if you look at the AD7124-4 eval board User Guide schematics, you will see they use the ADM1185 power sequencer to bring up IOVdd after AVdd.
Is a power-supply sequence recommended for power-up of AD7779 ?
In datasheet seems to be no requirement.
However, in EVAL-AD7779 evaluation board schematic, there is ADM1185 quad voltage monitor and sequencer.
From there looks that AD7779 analog supplies…
如果要控制各个电源轨的上电顺序的话,可能需要专用的上电时序控制芯片,如ADM1185/86等。关于第二个问题,帮您咨询一下产品线工程师。收到回复后,我们会马上回复您。
大家好,在做好的AD7656的电路板做测试时发现,在上电后AD7656工作之前,AD上输出的低电平波形是比较干净的,但是当给AD7656复位开始工作后,AD输出的低电平波形很差,毛刺很多,但是高电平输出是干净的,请问这是哪里出了问题。
这是画的电路图的一部分,电源模块没给出。其中模拟地与数字地之间是通过一个磁珠隔离开的。电源用了ADM1185、ADP1613(正负12V)、ADP3303、LM1117、ADP196。
Hello all. I have the following issue with AD7367: The current consumption on any power line (Idd, Iss, Icc, Idrive) is as expected when all power supply voltages are at normal operating levels (i.e. VDD=13V, VSS=-13V, AVCC=DVCC=5V, VDRIVE=3.3V). However…
The AD7768/AD7768-4 24 bit sigma delta ADC offers multiple power modes and decimation rates for scaling both power and bandwidth. There is also the option to use sinc or wideband filters and turn on or off analog pre-charge buffers, among many other configurable…