• ADM1176 4 in parallel with different supply voltage

    I am using 4 ADM1176 one for +3V3, one for +5V and two for +12V
    If I use +3V3 supply voltage for all of then or a combination of +3V3V and +5V for all of the, everything is working fine.
    when I move to of them to +12V they disappears on the I2C bus.
    It is…

  • ADM1176-2 reset

    I am using the ADM1176-2 (latching) part on a new PCB design.  I am wondering if setting the SWOFF bit over I2C can reset the latch state the same as toggling the ON pin?  The datasheet isn't entirely clear on this aspect--on Page 16 Table 11, it states…

  • ADM1176 TIMER pin high voltage

    I am currently using a ADM1176 on a custom board to protect the circuity ahead of it.  It was working at first, but something happened to shut off the GATE pin.  I measured the TIMER pin and read a voltage of 4.16V.  This seems to be quite high from what…

  • RE: ADM1176

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADT7420 (also ADM1176) - Need More than 4 on the same I2C channel!

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADI芯片辨识、型号查找

    看看截图: