Hello
One of the customer is considering to use ADM1075.
Referring to UG-548, there are ADuM5404 and ADuM1250.
The customer wants to reduce component count.
Then they are considering to reduce ADuM1250 and connect as below,
ADM1075
If would like to use ADM1075 usage 5 in a system that means I should use ADM1075-1 , ADM1075-2 in the same time here?
As I checked the datasheet that information below
DEVICE ADDRESSING
The ADM1075 is available in two models: the ADM1075-1 and…
Hi
I saw UG-304 Figure17 and 18.
ADuM1250 side1 is connected to ADM1075, I think.
Is it correct connection?
I think, a command trigger should be connected to side1.
Regards
moto
Jacky,
the ADM1275 simulation model is available at the product web page. The product page also has links to the EVAL board document with Layout examples as well as the software to run the ADM127x.
Hot Swap Controller Simulaton Model Simulation model…
The main difference between 1293/4's energy metering block and other similar parts from ADI is the energy count is now unsigned value instead of a signed value.
The ADM1293/4 has two energy meters monitoring power flow in both directions, which…
Good day!
This is Srinivasarao from Flex ,we would like to know the ESD levels for the parts mentioned .
HBM + CDM + MM etc.
MPN#