• VPx input impedance of ADM1069

    The ADM1069 datasheet revision C states at table 1 that VPx pins input
    impedance is 52 kohms. Based on my measurements and calculations it is 25
    kohms. In my experiment, VP3 is connected through 100kohm resistor to 5V.
    Voltage at VP3 pin is 1…

  • RE: Programming ADM1069

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADM1069 RAM update

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADM1069 EEPROM default value

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Restarting SE for ADM1069

    I'm having trouble getting the Sequence Engine for the ADM1069 to restart once I've programmed the SE and configuration register EEPROM.

    Essentially the goal is to run a script that can take an unprogrammed ADM1069 and program it and restart…

  • ADM1060 Power Sequencer support for USB interface

    Is there a USB programming tool for ADM1060 because parallel ports are no
    longer available on PCs. USB-to-Parallel adapters don't work as ADM1060
    evaluation SW can't redirect data for the ADM1060 to a virtual parallel port.
    Is there no…

  • RE: ADM 1069 first byte of EEPROM?

    Hi Ondrej,

    I tried reading back from the EEPROM after doing EEPROM erase, I'm reading back the correct data which is 0x20 (byte count) followed by 0xFF.....0xFF (since the EEPROM is erased). I also tried writing some data and read back the same data…

  • supersequencer installation error - missing dir/dll (supportfiles/customResource0009.dll)

    hi adi-folk.

    just downloaded the s/w tools for the adm1069 part.

    i first installed the "ADMxxxx Run-time Installer" ok, but when i try to install the the "SuperSequencer_EvaluationSoftware" on this win7 (all updates in) laptop, "setup" generates this…

  • RE: EVAL ADM1064TQEB documentation / manual

    Hi Karl,

    See attached for the user guide for this board.

    Ren