• ADM1063默认输出配置

    大家新年好,关于ADM1063,我在使用过程中碰到一些问题,具体如下:

    ADM1063数据手册中P18页的DEFAULT OUTPUT CONFIGURATION说明了在ADM1063出厂默认状态下,可以通过ADM1063片外的上拉电阻来控制PDO输出的电压,目前我们设计过程中图像处理芯片需要的电压分别为3.3V、1.8V、1.5V、1V_AVS、1V_CON。如果按照ADM1063片外上拉电阻来控制的话,是不是无法实现1V_AVS和1V_CON输出(Input supply = 0 V to…

  • How to reset the sequencing engine (ADM1063)?

    Hallo

    I  work on a project which includes basically a micro controller system and ADM1063 sequencing device. These two devices are connected by an i2c bus.

    My aim is to reset the sequencing engine of the ADM1063 while the system is running. Just turning…

  • ADM1060 Power Sequencer support for USB interface

    Is there a USB programming tool for ADM1060 because parallel ports are no
    longer available on PCs. USB-to-Parallel adapters don't work as ADM1060
    evaluation SW can't redirect data for the ADM1060 to a virtual parallel port.
    Is there no…

  • Use ADM1062's ADC from inputs VX1-5, VP1-4, VH & Temp sensor without averaging?

    Can I use the ADM1062's ADC from inputs VX1-5, VP1-4, VH and Temp sensor
    without averaging?
    I don't want to use the EEPROM for configuration. I want to initialize the
    ADM1062 every start up over the SMBus. Can you tell me which register…

  • ADM106x Headerfile

    Hello

    I´ve to program a ADM1062 for a project.

    And now my idea was to write a headerfile thats offer me the possibility to write something like

    VP1.PS1OVTH = 0;

    VP1.SFDV1CFG = 10US;

    Has someone allready made a headerfile with this definesor something…

  • how is EEPROM spaced being used on ADM106x and ADM116x family parts?

    how is EEPROM spaced being used on ADM106x and ADM116x family parts?

  • RE: EVAL ADM1064TQEB documentation / manual

    Hi Karl,

    See attached for the user guide for this board.

    Ren

  • 【ADI实验室电路合集】第2册PDF下载

    如题,灰常实用的资料。

    第一册在这里下载:【ADI实验室电路合集】第1册PDF下载:http://ezchina.analog.com/thread/6847

  • 分享ADI中文参考电路好资料,欢迎下载交流_01

    分享ADI中文参考电路好资料,欢迎下载交流_01