FAQ
Does Analog Devices have any data on the NSEU susceptibility of the ADM106x product line? Specifically what is the cross-section size of the registers? Are there any parity or error correction bits provided for the registers to flag when an upset occurred…
Hi,
ADM1062 does not have the certification to be used in medical application. Please refer to the ADM1062 datasheet for the specifications.
Regards,
Opal
Planning to use ADM1066 and its eval board. Here are 3 quick questions:
The USB-to-I2C dongle (USB-SDP-CABLEZ) terminates on a 10-pin Micro-Match
male connector. The connection to the Eval Board is via a 3-pin header, 0.1" pitch,
part number USB…