• ADL5902 CN0178

    Hi all,

    In the BOM list @ the ADL5902 CN0178, GCM1555C1H101JZ13D is obsoleted.
    MURATA is recommend to replace to the new part number, GCM1555C1H101JA16D.

    What part number is the replace part @ the ADI new board ?

    Best regards,
    sss

  • ADL5902 and highpass frequency (Formula 11)

    To whom it may concern,

    I doubt that formula 11 in ADL5902 Rev. B datasheet is correct.

    For a typical circuit, like Figure 45, in my opinion the resistance determing the high pass frequency is the ADL5902 input resistance and not the global input resistance…

  • ADL5902 VOUT information request

    I acquired an ADL5902 Evaluation Board for a prototype of RF Power Meter.
    The datasheet provided (ADL5902 Rev. B), shows graphics of OUTPUT VOLTAGE (V) vs. Pin (dBm) (Figure 3, 4, 5, 9, 10, 11, 15, 16). In SPECIFICATONS section, approximates this graphics…

  • RE: ADL5902 RF input impedance

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADL5902 at low frequencies

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADL5902 RMS Detector Noise Response

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADL5902 Vout calculation

    Hi ,

    I have doubt in calculating the Vout of ADL5902. I calculated Vout using this formulae (VOUT = VSLOPE × log10(RMS(RFIN)/VZ))

    Whereas Vslope=38.3mV, RMS(RFIN)= 223.607 mV(0dBm), Vz=0.8.

     

    For above assumption I expect output voltage  of 2.49V.but…

  • RE: ADL5902 vs. AD8312 vs. AD8362 or which?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADL5902 - Aging question: 0.8dB drift within 4 months.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Queries about ADL5902’s Response Time and Noise

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,