• ADL5811 connection with ADL5387

    In our design, we need to use both ADL5811 and ADL5387 evaluation board. Firstly, we would like to use ADL5811 evaluation board to convert the measured signal to an intermediate frequency IF. Then this IF signal is mixed down to I and Q signal by ADL5387…

  • RE: UPC2721GV similar part

    Take a look at ADL5801, ADL5350 or ADL5811.

  • Comment on FAQ: Calculating the Output Power of DAC/IQ Modulator Combination

    Do you have similar calculations done for ADL5811 mixer driving AD9255 ADC as predistortion receiver?

  • RE: Using ADL5391 to cancel antenna-to-antenna coupling in phased-array radar

    Hello Michael,

    I am trying to understand your application a little better so correct me if my understanding is incorrect.  You will be taking the output of the  AD8340 which has been amplitude and phase modified to generate the self-blocker-canceling signal…

  • RE: AD5811 & AD9255 gain calculations

    You can use the ADIsimRF tool to do these calculations. It has model data for ADL5811. It does not have model data for AD9255 but does have data on AD9254 which is a similar device. You can also type in data directly from the datasheet into this spreadsheet…

  • Comment on ADL5380 EVB中使用的巴伦

    有两种评估板可用,一个用于低频,一个用于高频。高频板上配有3600BL14M050。两种巴伦的尺寸相同。建议不要让RF和LO以单端方式工作,尤其是RF,因为你面对的是GHz频率,而且需要尽可能高的共模抑制。如果客户只能使用单端信号,我们有特别针对单端工作而设计的混频器,可帮助您实现最佳性能。请查看ADL5811/12。

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A