• ADL5802

    We would like to know regarding the evaluation board.

    We need to insert two RF signals differentially will it be possible.

    That is RF+ RF- to same mixer

  • ADL5802 overheating

    Hello,
    I have designed a receiver including ADL5802,


    1- I followed the datasheet, set enbl value to low, connecting it to ground through a cap.
    2- Setted the VSET to 3.3V taking it from voltage regulator.
    3- Used recommended minicircuits baluns etc.


    Aside…

  • ADL5802 datasheet

    The ADL5802 datasheet shows only the typical performance characteristics plots  with  an IF equal to 153MHz or 211MHz. Is the device capable of operation with an IF equal to 30MHz and is there any typical  performance data available?

  • ADL5801 or ADL5802 RF port common mode rejection

    Hello,

    is there some information available on the common mode rejection characteristics of the ADL5801 or ADL5802 RF input ports?

    With the V-to-I converter on this input, I suspect there can be some common mode rejection in the usable frequency band but…

  • Some Queries about ADL5802

    Hi, there


    i want to use ADL5802 for up/down conversion..

    i am having the following doubts regarding the ic

    1)since this IC has two independent mixers,can we use it in up conversion and down conversion mode simultaneously?

    2)could you please help…

  • ADL5350 ADL5802 upcovert performance ?

    Hi all,

    Out customer will select the upconvert mixer.

    ADL5350 and ADL5802 are included in the candidate device.

    The spec. and typical performance in the datasheet is downconvert measurement.

    Typical upconvert data is available ?

    Best regards,

    ss…

  • ADL5802 Eval Board

    Hi all, 

    I would like to know if the Eval board of the ADL5802 mixer, provides IF frequency range above 600 MHz. What is the range the eval board IF output is matched to?

    Thanks,

    Amin

  • ADL5802: Strom am Ausgang?!

    Hallo zusammen,

    habe eine Frage bzgl. des ADL5802.

    Weiß jemand zufällig, wie viel Strom maximal am Ausgang (OP1+/- und OP2+/-) fließt?

    Gruß

    Basev

  • ADL5802 downconversion to DC

    Hi,

    I would like to use the ADL5802 for downconversion to DC or frequencies of a few hundred Hz. From the datasheet I guess this is possible. Right? The output of the EVAL, however, does not seem suitable. How can I modify it. Can I simply remove the…

  • FAQ: ADL5802 Low Frequency Operation

    Q.

    The ADL5802 datasheet states that the device is capable of operation to  frequencies as low as 100 MHz, yet the Typical Performance  Characteristics plots only show data as low as 500 MHz. Is the device capable of operation at these low frequencies…