• ADL5801 or ADL5802 RF port common mode rejection

    Hello,

    is there some information available on the common mode rejection characteristics of the ADL5801 or ADL5802 RF input ports?

    With the V-to-I converter on this input, I suspect there can be some common mode rejection in the usable frequency band but…

  • I want to simulate the circuit of ADL5801 using ADS. Who will provide me the zap file of ADL5801 ? Thank you very much !!

    I want to simulate the circuit of ADL5801 using ADS. Who will provide me the zap file of ADL5801 ? Thank you very much !!

  • ADF4351+ADL5801

    Hi,

    I'm working with the ADF4351+ADL5801 project, in which the ADF4351 provides a 1.7 GHz LO for the mixer ADL5801. I referred to the Circuit Note CN-0239 which is attached with the message. In this circuit note, the two bias inductors L2 and L3 on…

  • Various questions/requests regarding the ADL5801

    Hello AD,

    I am planning to use the ADL5801 active mixer in a broadband application and have a request and a question.

    Request: Could you please post the S-Parameters for this device in the broadband raw configuration (with no RF or LO baluns) of Figure…

  • RE: ADL5801 bias connection, operation, and current consumption.

    A further question:

    Another "ADI Approved" post concerning the ADL5801 states:

    "Disable current is the current that the ENBL pin draws when the ENBL pin is pulled high. This pin typically draws 50mA when it is pulled high to disable the device…

  • AD9957+ADL5801

    AD9957评估板输出的中频模拟信号是否可以直接和ADL5801进行无缝连接,需要进行阻抗匹配吗?AD9957的输出阻抗是多少?

    谢谢!

  • AD9957+ADF4351+ADL5801

    Hi, everyone!

    I use AD9957+ADF4351+ADL5801 in an up-conversion application. The AD9957 generates a 50 MHz intermediate frequency signal which is sent to the RF port of the ADL5801; The ADF4351 provides a  1700 MHz LO, and the ADL5801 mixes the two signals…

  • ADL5801

    I want to use adl 5801 for my downconverter mixer...I want to give 5.8 GHz rf port and get 400 Mhz from IF port      and when I simulate s parameter of ADL 5801 and perfectly matching(Impedance tuner)  RF ports with using awr microwave office I get worst result…

  • ADL5801

    I'm looking to find s-parameters for this device.  I'm trying to use it at f RF~250MHz, f LO~70MHz.

    Thanks,

    Tim