• RE: SysParameters

    Hi Jim,

    The model for HMC1132 looks good and the data looks good when I run in a circuit.

    I have created an equivalent model for the ADL5611.  The ADL5611 does not correlate when I run it.  It looks like the model is extrapolating the last point in the…

  • RE: MAAM12000-Comparable MMIC

    I don't think that we have anything that can match this in a die form factor. For packaged devices, ADL5611, ADL5545 and ADL5523 are the closest matches. 

  • RE: BGA2709 similar part

    Nothing pin-compatible, there are alternatives in the industry standard SOT-89 package. Take a look at the ADL5545, HMC478ST89 or ADL5611.

  • Powering the new RF/IF gain blocks

    Can all of the new RF/IF gain blocks (ADL5544, ADL5545, ADL5610, ADL5611) be powered using a 9V supply through a dropping resistor?

  • RE: 100MHz to 4000MHz LNA

    Having to go that low in frequency, maybe better off with a low noise gain block like the ADL5611 or 5610.  Higher NF mid-band, but better behaved at low frequency (2.6 dB at 140 MHz for the ADL5610).

  • How should "de-embedded" block amplifier S-parameters be used?

    Specifically on gain blocks like the ADL5602 or ADL5611,  the file names for the S-parameter files all include the word "de-embedded."  To what point of the part is the de-embedding done (is it chip level or package level), or does this just mean…

  • RE: Pulse amplifier

    The ADA4960 is a bit of overkill costing about $15 and having only 1 GHz bandwidth and low gain and low voltage drive.   I was hoping to use something like the ADL5545 or ADL5611.    I had to purchase these to test them, and it would be oh so nice to have…

  • RE: ADL5322 RF Driver

    The ADL5322 is being phased out and not recommended for new designs. You can consider other RF driver offerings such as the ADL5320, ADL5324 or the HMC789ST89E for your application. These amplifiers need to be matched as described in the datasheet. The…

  • 6.5ghz amplifier

    hello,I use synthesizers that gives me 8 dbm output power,on 6.5ghz .I must amplify it to 20dbm to input it to a multiplier .of course

    it would be possible use a small power gaasfetbut I'd prefer to use a mmic.tHe circuit should simpler ,smaller and…

  • RE: RF Amplifer for Keysight Genesys

    The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys.  This library will be updated over time.

       

    PartNumber RealPartNumber Description