• RE: I have just started using an ADL5610 in an application. It exhibits a strange phenomenon where it draws too much current until I probe the input and then behaves as expected. There is no instability according to a diode detector on the input. The...

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADF5610 Maximum performance of RFOUT Power

    Could anyone clarify and give me any advice?

    Part : ADL5610
    Output Freq : 12GHz

    The best performance is the result of the datasheet,
    but What needs to be tuned in order to achieve better performance than the datasheet output?

    We want the maximum result…

  • ADF5610 EVB Setting....

    Could anyone clarify and give me any advice?

    Part : ADL5610
    Ref. Freq : 50MHz
    Output Freq : 10GHz

    According to U/G, ADF5610 EVB was tested.
    However, the result came out at 9.84 GHz. (Fig. 1)
    I don't know which one is the problem.
    We derive the same result…

  • RE: AD8354 recommended ground vias

    Thank you for your quick answer.

    I have an other question :

    Can you guarantee me that the device current does not have a pic current at the beginning?

    For example, the amplifier ADL5610 which has a current of 100mA has a pic current of 200mA when the…

  • RE: ADL5601

    please refer to the following link

    ADL5610 

  • RE: Distinguish POWER AMPLIFIER vs. DRIVER AMPLIFIER vs. GAIN BLOCK?

    Hi, Ntan,

        As you would expect, these are relative terms depending on the operating output power capacity (level) of the amplifiers, and one person's PA would be another's Driver.  Anyway, We looselycall anything above 1 W (dBm) a PA, and drivers…

  • RE: FMCOMMS3 driver for LTE and 802.11

    ok I understand.

    As a pre-amp, you can use the ADL5610.

    As far as PA goes, I am trying to find one for each of the output ranges you listed.

    Please stay tuned.

    Charly

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    北京市,海淀区上地三街中黎科技园1号楼,提供无线网桥/AP,关注ADL5610等

  • RE: 100MHz to 4000MHz LNA

    Having to go that low in frequency, maybe better off with a low noise gain block like the ADL5611 or 5610.  Higher NF mid-band, but better behaved at low frequency (2.6 dB at 140 MHz for the ADL5610).

  • 6.5ghz amplifier

    hello,I use synthesizers that gives me 8 dbm output power,on 6.5ghz .I must amplify it to 20dbm to input it to a multiplier .of course

    it would be possible use a small power gaasfetbut I'd prefer to use a mmic.tHe circuit should simpler ,smaller and…