• RE: RF power amplifier - ADL5604-EVALZ - query

    Hi Pradeepkka,

                               The ADL5604 EVB tuning will not perform at 1.4 GHz. You will need to develop a matching circuit for operation at 1.4 GHz. The de-embedded S-Parameters are available on analog.com.

    https://www.analog.com/media/en/simulation-models/s-parameters…

  • Biasing Circuit for  ADL5604

    I would like to design a power amplifier with the following specifications. Kindly let me know the part ADL5604 is suitable for this and also provide the biasing circuits.

     

    Freuqency band: 1500-1550 MHz

    Gain >= 10 db

    P1 dB  >= 28 dBm

    Output…

  • ADL5604/5606 Operating Current Specs

    Looking for the current specs on the ADL5604 and ADL5606 when in use. Could only find the quiescent current on the datasheet.

  • What is the IM3 of ADL5604

    Hi Sir,

    Could you provide the IM3 spec of ADL5604?

    Customer need to understand this parameter for design.

    Thanks!

  • FAQ: ADL5604 matching over a wide bandwidth

    Q: Can the ADL5604 be matched over a wide bandwidth?

  • 关于ADL5604匹配电路实现功率放大问题

    按照datasheet给的电路设计的是915MhzADL5604匹配电路但是芯片没有工作,为什么?设计的电路与DATASHEET上的2.4参考电路相比没有接入AD8009芯片,电容电感相对于芯片的距离是参考DATASHEET上给出的,只是把3号和4号引脚接到一起接到5V直流电源上,但是芯片没有工作,没有出现增益和功率放大,为什么?做了三片电路板都是这样的问题。  求解。

  • 关于ADL5604的电路设计以实现功率放大问题

    按照datasheet给的电路匹配参数设计的是915Mhz时ADL5604匹配电路但是芯片没有工作,为什么?设计的电路与DATASHEET上的2.14Ghz参考电路相比没有接入AD8009芯片,电容电感相对于芯片的位置是参考DATASHEET上给出的,只是把3号和4号引脚接到一起接到5V直流电源上,但是芯片没有工作,没有出现增益和功率放大,为什么?做了三片电路板都是这样的问题。 在ADS软件上的仿真电路结果S21参数等于21.3。  求解在不接AD8009芯片的情况下,3号引脚和4号引脚的正确接法…

  • 按照给的datasheet上参考图做的ADL5604驱动放大器电路为啥没有工作

    我设计频率是915MHZ,按照给的datasheet上参考图做的ADL5604驱动放大器电路为啥没有工作? 相对于官方给的评估板2.4Ghz时的电路图,如果不用AD8009芯片, 而且3号引脚和4号引脚的接法有没有谁知道正确的接法?   我把3号和4号引脚接到一起接到5V电源上,但是芯片没有工作,而且信号还衰减了20db,这是为啥?

  • RE: Query related to RF trnasceiver design

    Most transceivers have a maximum power output ranging from 0 to 13 dBm by design  -- many applications don't require more power than this and at higher  power levels the thermal limitations of the package and the  semiconductor process limit what's achievable…

  • RE: 频率转换功能IC

    您好!

    相关解决方案和产品请见附件内文档。