• ADL5601

    Hello

    Is it possible to use the ADL5601 with a biasresistor at an operating voltage of 9 Volt?

     
  • ADL5601

    I'd like to know if ADL5601 and ADL5610 amplifier are used as their evaluation board (without input and output matching) , can I  take into consideration that they are unconditional stable or can they oscillate?

    Best Regards

  • FAQ: ADL5601 Biasing

    Q: Can you provide the data when using ADL5601 with a bias resistor operating at 9 V?

  • ADL5601/2: Replacing Wirewound inductors with multilayer chip inductors

    Q. The ADL5602 datasheet recommends using a 470nH Coilcraft 0603LS-NX wirewound inductor for DC bias. Is it possible to achieve comparable performance with a Multilayer chip inductor, which tends to be cheaper than a wirewound inductor?

    ----------…

  • RE: RF Driver Amplifier (ADL5320) will it operate below 400MHz?

    Hi Rev.,

                  Internal circuitry prevents the ADL5320 from operating below 400 MHz.

      I suggest looking at the ADL5601, ADL5602, ADL5535 and ADL5536. the ADL5601 and ADL5535 are 15 dB gain blocks and will operate at 145 MHz. THe ADL5602 and ADL5536 are similar…

  • ADL5610

    I'd like to know if ADL5610 and ADL5601 amplifier are unconditional stable in the basic connection for operating show in their data sheet.

    Best regards

  • RE: Load Impedance ADL5565

    Hi Makkes,

    I would suggest you try using a single ended amp. The ADL5601 or ADL5602 might be a good choice for the amp. For Baluns checkout Anaren or Johanson.

    http://www.anaren.com/products/balun-transformers

    http://www.johansontechnology.com/integrated…

  • RE: AD9650 Evaluation Board ECB pattern data

    Hi TonyM-san,

    Thank you for quick reply.

    I will notify to my customer.

    I have two customers in one company.

    One group is designing RF receiver board by using AD9650-80 ADC and ADL5602, ADL5601, and FPGA.

    Another group is designing portable Spectrum…

  • RE: Query related to RF trnasceiver design

    To get from +5 dBm to +30 dBm, you will generally need two stages of amplification.  So in addition to the ADL5604 1 Watt amplifier that BobC recommends, also take a look at some lower power devices for your first gain stage.  Good choices would be ADL5601…

  • RE: RF Amplifer for Keysight Genesys

    The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys.  This library will be updated over time.

       

    PartNumber RealPartNumber Description