中文数据手册
技术文章
应用笔记
参考电路
CN0346
Hello Michael,
I am trying to understand your application a little better so correct me if my understanding is incorrect. You will be taking the output of the AD8340 which has been amplitude and phase modified to generate the self-blocker-canceling signal…
Hi Arnav,
You should be able to follow the user guide to get capture working with VisualAnalog (http://www.analog.com/en/design-center/advanced-selection-and-design-tools/interactive-design-tools/visualanalog.html). If you need to adjust any SPI settings…
Hi,
I followed the sample design given in fig 1 of CN-0227 circuit note of analog devices.
The filter design i cross checked with ADS solver. i am getting -13dB loss compared to 2dB loss claimed in the circuit note.
i have attached the screenshot of…
I am currently designing a frontend with the AD9650 as ADC. Due to the application, there can be interfering signals which are higher than the absolut maximum voltage of ADC for a short time. Recommended drivers like the ADL5562 can have a higher output…
Hello Lee,
If you operate the device within the specified range I do not believe you should blow up the part even across frequency. I see the slight discrepancy in the max rating power number as you had explained in your posting; however keep the power…
Actually, if you have the capability to use dual supplies, the AD8370 can be used as a dc accurate VGA. Using dual, symetric supplies, connect the VOCM pin and one of the inputs to gnd. This will set the internal bias point to 0V. I'm trying to find out…
Hi,
I took a look at the ADC Driver Selection Table and I have doubts about what would be the best fit for my application.
I will use a 105 MSPS - 14bit ADC sampling a 35MHz IF signal at 88MHz.
When I try to compare the Diff Amplifiers, I can see,…
Hi there,
As I mentioned in the title, I have an AD9467 adc and I want to drive it passively.
My first approach was like the Figure 51 on page 20 of the Datasheet.
http://www.analog.com/static/imported-files/data_sheets/AD9467.pdf
But when I analyzed…