• ADL5545

    I have an existing PCB that uses an ADL5536 (20dB gain at 500MHz). I need a pin-compatible part that provides at least 3dB more gain, 6dB would be ideal. The ADL5545 says it has 24dB gain, and do the plots in the datasheet. However, the S-parameter chart…

  • ADL5545

           最近准备做一个新设计,计划使用5545,但是发现datasheet里面的增益(24)与s参数描写不符合,差异达10dB请说明那个是正确的。

     

  • ADL5545 gain

    Hello,  I realize that the ADL5545 is spec'ed to 6 GHz but do you have any performance numbers to 7 GHz? 

    Thank you.

  • ADL5545, s-params

    Dear Sirs,

    For this gain block, are the s-parameters available let say upto 8GHz? On the web-page s2p-file is measured LF...6GHz.

  • ADL5545 & Keysight ADS

    Hi everyone,

    I am complitely new to board design and relatively new to ADS software, so my questions might be really basic.

    I need to design a board using Analog's ADL5545 gain block.

    I have seen that there are only .s2p files and .brd files of this…

  • ADL5545 Bill of Material

    Good morning,

    is it possible to have a BOM of ADL5545 amplifier? In particular, we have interested to implement the basic connection depicted in Figure 29 of datasheet for 100 - 500 MHz frequency band.

    Many thanks.

    Regards,

    Antonio L.

  • RE: Can you provide Residual Phase Noise Data for ADL5545?

    Hi Muttu,

                    We have nit measured  the phase noise for the ADL5545.We have measure phase noise for a similar part, ADL5544. Difference between the two is the ADL5544 has 7 dB less gain.

    Regards,

    Jim B

     PDF

  • ADL5545 datasheet and .s2p file

    Hi all,

    I am going to use ADL5545 to amplify a signal around 80MHz. 

    there are 3 locations that can find gain/return loss parameters, table 2 on page 5, picture 36/37 on page 16 and the .s2p file. 

    but they are different:

    parameter table 2 on page …
  • ADL5545 stability / DC feed question

    In the past other I have used MMIC amps have that either required a DC dropping resistor in the DC feed network or some form of a controlled current source to prevent damage to the device.  I am looking at using the ADL5545 in a new design and notice t…

  • [ADL5545] Using the deembedded S-parameters

    Good morning,

    On datasheet of ADL5545 amplifier (on page 5) we find a table that contains the s-parameters of component. Above the table, we read The effects of the test fixture have been deembedded up to the pins of the device.

    We are not understand…