• Could I get the load pull data of ADL5541?

    Dear ADI,

    Could I get the load pull data of ADL5541? Or Could I extract the load pull data of ADL5541 with ADS & ADL5541's ADS library?

    If these are not possible, then could I get the load pull data of any ADI RF amplifier?

    I would like to compare…

  • 12/16/2015: Full RF Signal Chains from 0Hz to 110GHz

    Presenter: Mel Conway, Product Manager, Instrumentation, High-speed & RF and Precision

     

    This webcast will explain ADI's new and expanded RF capabilities since the acquisition Hittite Microwave. We will give examples of the wider frequency spectrum…

  • RE: 频率转换功能IC

    您好!

    相关解决方案和产品请见附件内文档。

  • RE: what is the Phase Noise and Spurious performance between ADF4150 and ADF4151 ? which one is better? I planned to use upto 3GHz...

    If you want to improve PFD spurs, you can use the VCO output while working with ADF4150 and put a buffer between VCO output and RF input of the ADF4150 (please refer to the User Guide UG-380: http://www.analog.com/static/imported-files/user_guides/UG…

  • 【在线研讨会讲义PPT下载】从0Hz到110GHz的全频谱RF信号链

    此次在线研讨会阐释了自收购Hittite Microwave后ADI的全新及扩展的RF能力。我们会举例说明ADI涵盖的更宽频谱范围及其真DC的重要性。信号链外的性能同样至关重要,展示低噪声、高稳定性控制和电源元件如何改善总体RF信号性能,并将讨论完整的信号链示例。

    主要讨论天线到比特和比特到天线,信号链覆盖,即刚才提到的从真正的DC 0 Hz到110 GHz的频谱覆盖。 我会简要介绍其中涉及到的各类设备。

    为什么良好的RF需要良好的电源,大家知道,RF需要干净的电源。然后,最后会和大家讨论“不止是芯片…

  • RE: ADF4350 in local oscillator application

    Hi Rich,

    1. The modulus is related to the channel spacing or frequency steps. Gory details on how to calculate are in the ADF4153 etc. fractional N data sheets.

    So as you step through channels you step through N, N+1, N+2 etc divided by the modulus…

  • RE: ADF4193 Does Sim PLL predict integer boundary spurs

    ADIsimPLL models fractional spurs but not integer boundary spurs which are caused by a separate mechanism, namely

    interaction between the RF and harmonics of the reference frequency. The ADF4193 datasheet talks about one method to avoid integer boundaries…

  • RE: RF Amplifer for Keysight Genesys

    The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys.  This library will be updated over time.

       

    PartNumber RealPartNumber Description
  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • AD-MSDPD-EVB: Eval Board Datasheet

    I am not able to find the datasheet of the AD-MSDPD-EVB

     

    please find attached

    The Board is not longer available to the public
    Attachments: