Hello,
We have ADL5536 evaluation board, and as per datasheet , there is a flat gain over the band of DC -1 GHz, but at our required frequency 466.8 MHz , gain is 13 dB instead of 18 dB, please provide suggestion.
Hello,
We have ADL5536 evaluation board, and as per datasheet , there is a flat gain over the band of DC -1 GHz, but at our required frequency 466.8 MHz , gain is 13 dB instead of 18 dB, please provide suggestion.
1.ADL5536在1.5G能达到15dB的增益吗?
2.ADL5536在1.5G的版图是按照1880-1990MHz的评估板绘制么?
3.ADL5536的手册里说,C3的位置影响很大,但是C3的位置并没有给出确定的值,是不是只要在隔直电容之前就可以了
I mean, if I have a bipolar signal, ADL5536 will work on both cycles or it will work only in positive? What happens if it works in negative voltage?
Thank you.
Hi, I need have implemented a test board with two ADL5536 gain blocks to achieve a signal gain of 40dB. Each individual amp works well, however when I link the two the board becomes unstable and oscillates at about 800MHz.
I have used 100nF input/output…
Hi,
In considering these parts for a design, while they have specified (and very good) IP3 specs, the application requires understanding IP2 as well.
Can you please share IP2 data? It's not spec'd in the datasheets.
Thanks
Dear Supporter,
When ADL5536 power on ,we need to wait 100~200us to transmit data. If we don’t wait 200us , we receive incorrect amplitude signal level at RX.
Is this test result correct?
Could you please help provide the power on timing if possible…
I required model file of ADL5536 for simulation.If any one has pspice or any kind of file of ADL5536 for simulation,please share it.
Hello Supporters,
We are planning to use the amplifier ADL5536, for the frequency range of 20-1000MHz, as LNA for wide-band receiver. For finalizing the part we need the stability factor for the same over the frequency range of 20-1000MHz or any information…