• ADL5535 as ADC Driver

    Hello,

    I am trying to drive an ADC with a high impedance differential input by using two (single ended) ADL5535 amplifiers to serve as the differential input. A few questions:

    1. Is it wise to use two amplifiers in this manner or should I stick to using…

  • ADL5535 1PdB - 1dB Compression Point Unterstanding

    Hi Folks,

    please could you help me to explain the fact, that the ADL5535 has a higher 1dB compression point than the power supply allows?


    Example:

    1dB P1 = 18.6dB as lowest in statistic, according to Fig.11. of the datasheet.

     

    18.6dB is 72.44mW…

  • Is ADL5535 designed for a specific output power?

    I called in to ADI's tech support asking why I was getting less OIP3 than what is stated in the specification section in the datasheet and was pointed to figure 7 on page 8 showing OIP3 versus output power.  I see there a significant spike in OIP3…

  • Operating the ADL5535/6 with a lower value of choke inductor

    Q. The ADL5536 recommends a 470nH choke inductor value for optimal performance? Can the device be operated with a lower value of inductor?

    ------------------------------------------------------------------------------------------------------------…

  • RE: RF Driver Amplifier (ADL5320) will it operate below 400MHz?

    Hi Rev.,

                  Internal circuitry prevents the ADL5320 from operating below 400 MHz.

      I suggest looking at the ADL5601, ADL5602, ADL5535 and ADL5536. the ADL5601 and ADL5535 are 15 dB gain blocks and will operate at 145 MHz. THe ADL5602 and ADL5536 are similar…

  • RE: HMC313 output matching w/Evaluation Board

    Hi sss@jpn,

    The layout for the original EVB was not correct in my opinion. It had a T-stub inductor connection, when the bias inductor should really land on the output line.

     We recommended something similar to the ADL5535 layout (linked below).

    https…

  • 仿真模型找不到

    为什么在ADIsimPE中找不到ADL系列的仿真模型,比如ADL5535,。

    而且请问

    ADISimPE和ADISimRF,ADISimPLL三者有什么区别

  • Understanding of OIP3

    Hi

    I have a question about OIP3 of ADL5535.
    Datasheet says that OIP3 is 45.5dBm at 190MHz and 380MHz. Is this indicated as the total power of two-tone ?
    And the attached file shows my understanding.
    Please find attached file, and let me know my underst…

  • RE: ADL5320 lamdba values

    The Lambda values for frequencies from 400 MHz - 500 MHz and 800 MHz - 960 MHz,are shown on page, 15, of the ADL5320 datasheet. Application circuit development focused on  the major communication bands.   

    S-Paramters are available via download so the end…

  • RE: RF Amplifer for Keysight Genesys

    The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys.  This library will be updated over time.

       

    PartNumber RealPartNumber Description