• ADL5523 failure

    Hello,

    I met several cases of ADL5523 failures which is characterized by over current consumption of 200mA on power input (sooner a short circuit...).

    This component is power by a LDO generating 3.3V from USB 5V.

    Without considering potential over voltages…

  • ADL5523 switch on time

    We are using the ADL5523 in a TDMA application as an LNA. Is there a specification for the switch-on time? I didn't find anything about timing in the data sheet.

  • ADL5523 Maximum Input Power

    Hello,

    I am interested in if the maximum RF Input Level of 7dBm is valid even if the device is unpowered. There are cases in my application where we will be unpowered but still connected to the antenna and I want to make sure the part is still rated to…

  • ADL5523

    Hello

        I have a question about the ADL5523 evaluation board. Can you tell me how to modify the evaluation board to work at any frequency between 400MHz and 4GHz? I want to know  the suitable value that adl5523 can work at 400MHz to 500MHz.

        Thank you…

  • RE: ADL5523 S parameters simulation

    Hi Bruno,

    If you mean like default eval board, yes it is 1950 MHz.

    Regards

    Ivan S

  • RF-ADL5523

    Hello, I want to design a bandpass amplifier with a bandpass frequency between 400MHz and 500MHz. I use the ADL5523 as the amplifier chip,and i hope you can give me some suggestion about the ADL5523 chip. I want to know if the ground resistance can be…

  • RE: about ADL5523

    Hello! Remove the capacitor 0.5 pF, connected between the input and ground, at the amplifier input.

  • RE: ADL5523

    Hi,

    We currently do not support spice model for ADL5523.

    Regards,

    David

  • RE: ADL5523  How to 3ports matching

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADL5523 and eval board set up

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,