Hi,
Do you perhaps have any data on image rejection for higher IF frequencies? Specifically around 250 MHz, while the RF frequency is 5250 - 5750 MHz. If you have data for both high-side and low-side LO that would be great.
Thanks
Hi,
Do you perhaps have any data on image rejection for higher IF frequencies? Specifically around 250 MHz, while the RF frequency is 5250 - 5750 MHz. If you have data for both high-side and low-side LO that would be great.
Thanks
Hi David,
I need your help.
I am testing the new Eval board of ADL 5380 .
I have done all the necessary changes told by you for the operating frequency 5.81Ghz at Lo and Rf like
1. Removed R13 to R16
2. Populated R2 to R5 with 0 ohm
3. Populated R6 and…
大家好,调研了一些调制解调器,看应用里面都没有写5GNR的情况,请问一般IQ调制解调器支持5GNR信号的应用吗?
下图为官网LTC5588-1的应用介绍:
Q:
Is the performance of the ADL5380 maintained below 400 MHz?
-------------------------------------------------------------------------------------------------------
A.
The minimum frequency as specified on the ADL5380 datasheet is 400 MHz. Performance…
We have the eval board of ADL5380. We desire to operate it in a single-ended mode. As suggested in the datasheet the RF and LO input already has a 100pf capacitor connected to one port and ground on the eval board for single-ended mode. According to the…
Re: ADL5380 DSB NF Measurement by Qui
Hello HJ,
A standard agilent NF meter (like the N8974A) by its nature is measuring DSB. In the case of the ADL5380 the DSB number of one channel (I or Q) is measured and reported. Because the ADL5380 is an I/Q demod…
Good Evening Sir/Madam,
We bought ADL5380 EVM from Analog Devices.
Practical Observations
1. As per datasheet, this EVM provides 7dB insertion loss at 900MHz, but we observed that ADL5380 is providing 30dB insertion Loss.
2. This EVM is providing insertion…
Q.
What is the 1/f noise of the ADL5387
-------------------------------------------------------------------------------------------------------
A.
Attached is the 1/f noise of the ADL5380. I had a discussion with the design engineer of the ADL5387…
Hello EZ Team.
My customer has a question regarding ADL5380 EVM dependence vs input signal. They have calculated some parameters using ADISimRF as well as MathCAD. Calculations show that linear EVM degradation is caused by the demodulator noise floor…