• FAQ: How can I avoid startup transients when operating the AD8318 in Controller Mode?

    Q.

    How can I avoid startup transients when operating the AD8318 in Controller Mode?  I am using the AD8318 Log Detector/Controller to control  the output level in an AGC loop.  The control loop consists of a fixed-gain  RF amplifier, an ADL5330 VGA, a…

  • Balun

    Hello,

    I have a doubt about how to use the baluns. I have seen in aplication notes that, in the evaluation boards, if you have a SMA conector (like an input or output to the PCB) it's used the balun to convert the unbalanced input (ANNTENA) to a balanced…

  • ADL5330 Impedance Data

    Hi,

    Is there impedance data available for the ADL5330 VGA?

    We are using in the front end of a 450 MHZ radar system

    Thanks,

    Ed

  • AD8317 operation at 10GHz & impedance matching

    Hello,

    I am interested in using the AD8317 log amplifier at 10GHz.  The AD8317 is specified for operation up to 8GHz, but can be used up to 10GHz with a reduced dynamic range.

    The datasheet (page 15) states that implementing an impedance match for frequencies…

  • RE: HMC993 replacement part for AGC circuit

    Hi Vincent,

    Thanks for your inquiry.  We have other VGA and Detector products that may work for your application.  A couple of analog devices that may apply are:  ADL5330 analog VGA and a log detector, AD8318 .  Details are available on Analog.com.  See also…

  • ADL5330 and AD8318 AGC circuit

    Hi Experts,

    I used ADL5330 and AD8318 to configure AGC Loop.

    The circuit is same as Fig37 in page16 of ADL5330 spec.

    In CW mode, it works perfect.

    I have a question, if I want to use it in pulse mode.

    Carrier is 500M, the pulse width is 100ms…

  • ADL5330 ENBL pin control w/ RF power input

    Hi all,

    About ADL5330,
    hot swiching (on/off control) of the ENBL pin is available with the RF signal input @-10dBm ?

    Best regards,
    sss

  • BOM list of ADL5330 evaluation board

    Hi

    Could I have the BOM list of ADL5330 evaluation board?

    Especially, I want to know coil vendor and parts# of  L1A, and L2A .

    Regards

    moto

  • RE: ADL5330 Gain Setting

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADL5330 pin connections.

    Hi ,

    Is it possible for me to know the Gain in dB vs Control voltage relation( mathematical expression ) in ADL5330

    Does Analog devices provide any ADS model of the device

    Thanks