ADL5324在1.5GHz处参数手册并没有给出它的匹配电路。按照1880MHz的参考电路设计,只有10dB的增益。请问ADL5324的1.5GHz匹配电路是什么呢?能否给出负载牵引图与1.5GHz的匹配电路参考设计
Hi Everyone,
ADL5324 is 400MHz - 4GHz. S parameters provided in documents in web is 10MHz - 600MHz.
How can I have the s parameters for entire band which is 400MHz - 4GHz.
I have checked before posting the question, I couldn't find info, so a new post…
The S-Parameters provided in table 2 are the S-Parameters for an unmatched device. ( the ADL5324 requires external matching in order to be used) When the part matched using the recommended matching components listed in table 6 and placed at the recommended…
I want to use the driver amplifier IC ADL5324 for my RF design. The reference layout is given on four layers but I want to design it on a two layer PCB. Are there any changes/caution required designing it on a two layer PCB?