Hello Support team,
Can I get a spice model of ADL5324 ?
I know there is a S-parameter in adl5324 product page, but I need a spice model.
Thanks.
Hello Support team,
Can I get a spice model of ADL5324 ?
I know there is a S-parameter in adl5324 product page, but I need a spice model.
Thanks.
Hi,
In the ADL5324 datasheet there are reference designs and layouts.
On page 19, figure 17, the layout for the 3500-3700MHz operation. There is a series inductor on the output, L2.
It is 4.7nH.
At 3500MHz, this gives a reactance of 103 ohms.
Considering…
Hi,
I am having an application in which I am going to use 400 - 420 MHz band. Design is based on a 3.3V supply. Reference designs in the data sheet is given for 420 - 494 MHz band. Will there be any change in component selection from the reference design…
Hello ,
I have purchased a default eval board of ADL5324 as per below link and data given, this eval board works quite well in the 2.2 GHz to 2.3 GHz
ez.analog.com/.../3704.ADL5324-2p2_2D00_2p3GHz.xlsx
But, data does not match with our purchased default…
I would like to use the ADL5324 with a transceiver to achieve greater range, I know my power output would be above regulations but this is not for regular use or making a product that I would distribute. It is for a school project and purely as a proof…
Hello,
Can you please provide FR4 material dielectric thickness used for ADL5324-evalz board?
What should the component matching distances be for a 1GHz square wave? The data sheet lists 869-961MHz but then nothing until 1880MHz by which time the distances have reduced considerably.Do I assume 1GHz is close enough to 961MHz ?
I don't have access…
Hello sir,
I have purchased ADL5324 default eval board, But it does not provide the same gain and return loss in between 2.2 GHz to 2.3 GHz as per above attached excel data.
Please check measurement of the default eval board I have attached here. VCC…
Hi,
I'd like to know the maximum VSWR the ADL5324 amplifier can withstand without permanent damage.
Thanks a lot.