• Pulsing Vcc for ADL5321


    I would like to power up and power down the ADL5321 quickly in order to save power in my system. I only need the device to be operational for 10-20ns at a time, then powered down for many microseconds. The faster the switching time, the more power I can…

  • ADL5375-05 Pulse Mode

    In my application modulator uses in pulse mode with ratio 1:10.

    What do you think if to power off modulator and amplifiers (ADL5321) for 900 us and power on for 100 us?

    Practically I found out that after 2 us of power on modulator is able to work fine…

  • 6.5ghz amplifier

    hello,I use synthesizers that gives me 8 dbm output power,on 6.5ghz .I must amplify it to 20dbm to input it to a multiplier .of course

    it would be possible use a small power gaasfetbut I'd prefer to use a mmic.tHe circuit should simpler ,smaller and…

  • RE: RF Amplifer for Keysight Genesys

    The attached list details all of the ADI RF Amplifier Sys-Parameter models that are available in the 2015.08 release of Keysight Genesys.  This library will be updated over time.

       

    PartNumber RealPartNumber Description
  • RE: Query related to RF trnasceiver design

    To get from +5 dBm to +30 dBm, you will generally need two stages of amplification.  So in addition to the ADL5604 1 Watt amplifier that BobC recommends, also take a look at some lower power devices for your first gain stage.  Good choices would be ADL5601…

  • 五类放大器的基本特性

    LNA(低噪声放大器)、IFA(中频放大器)、驱动器放大器、增益模块和VGA(可变增益放大器),他们的基本特征你都掌握了么?

     

    低噪声放大器

    低噪声放大器(LNA)通常用作接收路径中的第一个有源元件,它是界定系统总体性能的关键元件,必须能在不显著增加噪声的情况下成功放大极低的电平信号。选择LNA时需要考虑的一个重要特性是噪声系数,该系数与放大器增加到输入信号中的噪声量有关。P1dB和OIP3也很重要,前者与放大器可以输出的线性信号功率量有关,后者与功率处理能力,即放大器能够处理而不会受到损害的输入功率量有关…

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • RE: ADI的RF放大器能不能应用一下范围

    您好!

    ADI工作于2.4GHz频段的射频放大模块产品有很多,请见附件内表格,供您参考。

  • AD-MSDPD-EVB: Eval Board Datasheet

    I am not able to find the datasheet of the AD-MSDPD-EVB

     

    please find attached

    The Board is not longer available to the public
    Attachments:
  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF