• ADF4360-7的频率不改变问题

    8b2c970a89270699cce2d2cd6ae72cc3.html

     我用ADF4360-7做一个多频率输出的电路(在RFOUTA后接入了2级的ADL5320的放大 RFOUTB接50欧的电阻接到地。也就是说我只想用一路输出,另一路输出通过50欧的电阻匹配连接到地,不知这样是否正确)。按资料说明改变R、C、N寄存器可以改变输出频率。 我上电后按程序分别写入计数器在频谱仪上观察得到一个信号强度在10dbm左右的400M 频率。而且无论我如何改变寄存器的值…

  • RE: ADI的RF放大器能不能应用一下范围

    您好!

    ADI工作于2.4GHz频段的射频放大模块产品有很多,请见附件内表格,供您参考。

  • 五类放大器的基本特性

    LNA(低噪声放大器)、IFA(中频放大器)、驱动器放大器、增益模块和VGA(可变增益放大器),他们的基本特征你都掌握了么?

     

    低噪声放大器

    低噪声放大器(LNA)通常用作接收路径中的第一个有源元件,它是界定系统总体性能的关键元件,必须能在不显著增加噪声的情况下成功放大极低的电平信号。选择LNA时需要考虑的一个重要特性是噪声系数,该系数与放大器增加到输入信号中的噪声量有关。P1dB和OIP3也很重要,前者与放大器可以输出的线性信号功率量有关,后者与功率处理能力,即放大器能够处理而不会受到损害的输入功率量有关…

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A
  • ADI专家面对面之五——ADI产品介绍及其在各个领域中的应用

    ADI专家面对面是ADI公司与广大中小型客户以研讨会和客户拜访的形式直接交流的活动。ADI技术专家现场指导客户如何应对实际设计应用中面临的问题,并详细讲解了用户在实际应用中遇到的常见问题和解决方法。

    应广大客户的要求,我们将陆续上传ADI资深工程师们在研讨会现场的演讲PPT,以供大家参考,学习与探讨。

    目前更新至第五场研讨会的内容。

    第一场与第二场内容:深度了解168通道同步采样数据采集系统AD7606

    第三场内容:深入介绍放大器应用与经典案例分析

    第五场内容:ADI产品介绍及其在各…

  • RE: ADL5385 Output Level and LO Drive

    It is good to hear that the output power of ADL5385 is now normal. In terms of EVM, please check LO Leakge level which is also related to EVM performance. If possible, you can get better EVM by nulling LO Leakage level. Refer attached file for correcting…

  • RE: I and Q not 90-degrees apart (AD9854)

    Hi Matthias,

    Thanks for your answer, it was very detailed and most helpful. I'd come to the same conclusiion that I and Q outputs are fixed at 90-deg and no trimming is possible although I was hoping I'd missed something in the DDS datasheet. It does…