• ADL5202

    Hello,

    Could you please tell me what are the default ( power on ) values for the registers in the ADL5202? Thanks.

    Best Regards.

  • ADL5202 Measurement

    Hello,

    For ADL5202(WVGA),

    I wonder how to test CMRR and Slew rate of ADL5202.

    and plz recommend the test configuration.

    Best regards,

  • ADL5202 STARTİNG GAIN VALUE

    I use ADL5202 amplifier in my project but I don't have any pin to control gain configuration. What's the starting gain value exactly for ADL5202?

    Thank you for your attention.

  • What is the input capacitance of VINA+ and VINA- pins of ADL5202?

    Hi,

    Although I have thoroughly search the datasheet of the ADL5202, I could not reach any information about input capacitance of VINA/VINB pins. Also, I am trying to send signal at 10 MHz from ADA4950 to ADL5202. My main concern is ability of ADA4950…

  • RE: Input capacitance of VINA/VINB pins of ADL5202

    Hi Ekin,

    The input capacitance for the VIN pins is not in the datasheet as you indicated, the best source for this information would be the sparameters. These are located on the ADL5202 webpage to download.

    http://www.analog.com/en/products/rf-microwave…

  • ADL5202 CMRR Test

    Thank you for the reply for last question.

    I have one more question for CMRR.

    I tested the CMRR using the ADL5202 Evaluation board as below configuration a few days ago.

    But, I could not get the similar result of Datasheet of ADL5202 for CMRR.

    Please…

  • RE: ADL5201 or ADL5202 in cascade configuration

    This is a duplicate thread. Go to this link ADL5201 or ADL5202 in cascade configuration for details and answers.

  • RE: ADL5201 or ADL5202 in cascade configuration

    This is a duplicate thread. This question is answered in this link ADL5201 or ADL5202 in cascade configuration.

  • RE: ADL5201 or ADL5202 in cascade configuration

    This is a duplicate thread. Refer to this link ADL5201 or ADL5202 in cascade configuration for information and answers.

  • Windows 8 drivers for ADL5202-EVALZ

    Hi there,

    Is it possible to get Windows 8 drivers for ADL5202-EVALZ?

    Thanks